For 100 Years
Proud to serve our customerS
Featured Products
Overview
Product Offerings
Resources
FAQs
Manufacturing Reliable and Rugged Products
Since 1924
A manual battery disconnect switch (also known as a battery cutoff switch, battery isolation switch, or battery shutoff switch) is installed…
Connect with Us
Littelfuse, Inc. 6133 North River Road, Suite 500, Rosemont, IL 60018 USA, 773-628-1000 Copyright © 2025 Littelfuse, Inc.
Overview
The Cole Hersee brand has been a pioneer and leader in the development of heavy-duty electrical products for the vehicle industry – collaborating on many industry standards and earning a reputation for quality and value.
In 2010, Cole Hersee became part of Littelfuse. This strategic acquisition not only strengthened Cole Hersee’s capabilities but also extended its reach and resources. Under the Littelfuse umbrella, Cole Hersee continues its legacy of excellence while also innovating and expanding its product lines.
As we celebrate 100 years of innovation, dedication, and success, the Cole Hersee name continues to stand for quality, reliability, excellence, and forward-thinking solutions.
Product Offerings
Battery Disconnect Switches
An extensive series of ignition switches that can also be used as rotary switches. Suitable for a broad range of voltages: 10A at 12V, 5A at 24V…
95060-50
The 36 V 85 A Continuous-Duty SPST Series Insulated Solenoid Relay (24059) is designed with
a plated steel housing, single-pole, single-throw (SPST)…
24059
With a patented weld breaker safety feature and integrated lockout/tagout, the 75930-Series Battery Master Disconnect Switch…
75930
NEW
New and Featured Products
View More
View More
DC solenoids are relays used for remote switching of electrical currents from 20A to 600A. Littelfuse offers a variety of DC solenoids and relays…
Solenoids and Relays
View More
User-operated switches that Littelfuse produces for commercial vehicles, farm equipment, material handling, and heavy equipment…
Control Switches
View More
Battery management devices provide various methods of conserving starting power, protecting against over-discharge, combining power from…
Battery Management
View More
Automotive busbars and terminal blocks allow you to consolidate wiring and distribute electrical power in a cost-effective manner. Busbars…
Busbars & Terminal Blocks
View More
Rely on our LED and incandescent panel lights and pilots lights to alert you when a piece of equipment starts, stops, or requires maintenance…
Indicator Devices
View More
full range of connectors for commercial vehicles and farm equipment. Our high-performance, innovative products for 12 V and 24 V applications…
Vehicle Connectors
Battery Disconnect Brochure
Featured Resources
View
Relays Brochure
View
View
Transportation Product Catalog
View
Commercial and Fleet Application Book
View
Mining Guide
IP Rating Info Sheet
It’s a quantified measurement of a given switch’s ingress protection. The IP rating will tell you how “waterproof” a switch is and how resistant it is to the ingress of dust.
What is an IP Rating?
View More
Sometimes, items such as solenoids and illuminated switches must be used at the rated current and voltage due to the internal components. Ignition, push-pull, …
Can Cole Hersee products be safely used in 24V applications?
View More
Although some manual battery disconnect switches are push-button emergency cutoff switches, in most cases, manual battery disconnect switches are rotary switches …
How do manual battery disconnect switches work?
Sometimes, items such as solenoids and illuminated switches must be used at the rated current and voltage due to the internal components. Ignition, push-pull, momentary, door and other types of non-illuminated switches can be used in a 24V system, with one provision. For a 24V application, you must de-rate the current capability of a 12V product.
De-rating: using Ohm's Law, if you double the voltage, you must divide the current in half. For example, if you have a 12V, 20A product, you can use it in a 24V, 10A system. You cannot use lighted switches at different voltages than those specified.
View Less
Although some manual battery disconnect switches are push-button emergency cutoff switches, in most cases, manual battery disconnect switches are rotary switches with lever, handle, key, or knob actuators. They may be single-pole, single-throw (SPST) switches for simple on/off functionality, dual-pole, single-throw (DPST) switches, or even single-pole, triple-throw (SP3T) battery selector switches for vehicles that use an auxiliary battery.
View Less
View More
A switch with a higher rating will have more expensive internal components (bronze, copper, silver, and sometimes gold)...
View Less
A switch with a higher rating will have more expensive internal components (bronze, copper, silver, and sometimes gold). Therefore, the cost is higher. Always select a switch that meets or slightly exceeds your needs. Failure to do so could lead to you paying for extra capability that you don't need or you ending up with a switch that fails because it doesn't meet your specifications. Cole Hersee offers a broad range of switches in different current ratings to allow you to buy the product that best suits your needs at the best price.
Two switches in the Catalog look identical, but one has a higher current rating and costs more. Why?
View More
Sometimes, items such as solenoids and illuminated switches must be used at the rated current and voltage due to the internal components. Ignition, push-pull, …
View Less
Sometimes, items such as solenoids and illuminated switches must be used at the rated current and voltage due to the internal components. Ignition, push-pull, momentary, door and other types of non-illuminated switches can be used in a 24V system, with one provision. For a 24V application, you must de-rate the current capability of a 12V product.
De-rating: using Ohm's Law, if you double the voltage, you must divide the current in half. For example, if you have a 12V, 20A product, you can use it in a 24V, 10A system. You cannot use lighted switches at different voltages than those specified.
Can Cole Hersee products be safely used in 24V applications?
Frequently Asked Questions
View More
Although some manual battery disconnect switches are push-button emergency cutoff switches, in most cases, manual battery disconnect switches are rotary switches …
View Less
Although some manual battery disconnect switches are push-button emergency cutoff switches, in most cases, manual battery disconnect switches are rotary switches with lever, handle, key, or knob actuators. They may be single-pole, single-throw (SPST) switches for simple on/off functionality, dual-pole, single-throw (DPST) switches, or even single-pole, triple-throw (SP3T) battery selector switches for vehicles that use an auxiliary battery.
How do manual battery disconnect switches work?
The Cole Hersee brand has been a pioneer and leader in the development of heavy-duty electrical products for the vehicle industry – collaborating on many industry standards and earning a reputation for quality and value.
In 2010, Cole Hersee became part of Littelfuse. This strategic acquisition not only strengthened Cole Hersee’s capabilities but also extended its reach and resources. Under the Littelfuse umbrella, Cole Hersee continues its legacy of excellence while also innovating and expanding its product lines.
As we celebrate 100 years of innovation, dedication, and success, the Cole Hersee name continues to stand for quality, reliability, excellence, and forward-thinking solutions.
The Cole Hersee brand has been a pioneer and leader in the development of heavy-duty electrical products for the vehicle industry – collaborating on many industry standards and earning a reputation for quality and value.
In 2010, Cole Hersee became part of Littelfuse. This strategic acquisition not only strengthened Cole Hersee’s capabilities but also extended its reach and resources. Under the Littelfuse umbrella, Cole Hersee continues its legacy of excellence while also innovating and expanding its product lines.
As we celebrate 100 years of innovation, dedication, and success, the Cole Hersee name continues to stand for quality, reliability, excellence, and forward-thinking solutions.