Littelfuse Empowers Engineers
When it comes to building automation solutions, Littelfuse products empower engineers to design cutting-edge products for a safer, connected, and more sustainable world.
Learn more about Littelfuse solutions
with the
Building
& Home Automation Application Guide.
In the last few years, there has been a
widespread shift in the use of automated
and smart technologies in commercial
building design. Driven by increased energy and environmental regulations, as well as increased safety and convenience factors, commercial spaces are becoming hubs for technology.
Click through
Smart Locks
Door & Window Sensing
Outdoor & Wireless Security Cameras
USB Outlets
Smart-Lighting
GFCI/AFCI Receptacles
Intelligent Outlets
Electronic Dimmers
Electric, Gas, & Water Meters
PIR Motion Detection
Smart Thermostats
HVAC Systems
Elevator & Escalator Systems
to take a tour of a typical
Littelfuse is at the forefront of this growing market, creating solutions that are ideally suited for commercial automation applications.
Smart Locks
Smart-lock technology ensures access to specific rooms or buildings only to those who should have it. With a wireless interface, users can access the lock either locally via smartphones or remotely via a network-attached PC.
TVS Diode Array
Littelfuse at Work
Proximity detection to verify that door properly closes
Reed Switch
Door and Window Sensing
Open doors or windows not only present potential security concerns but also impact energy efficiency, causing heating and cooling systems to needlessly run. With door and window position-sensing systems, the status of doors and windows can be remotely monitored and users can be alerted when a door is left ajar or a window opened.
Littelfuse at Work
Outdoor and Wireless Security Cameras
Advancements in wireless technology have also made wireless security cameras a more reliable standard, even with high-definition video. Littelfuse technology helps keep these security-critical devices protected.
Littelfuse at Work
USB Outlets
Modern businesses are run on the go — and that means smartphones and tablets are a necessity. As such, many commercial spaces are incorporating USB outlets into their design. USB outlets combine traditional AC wall outlets with USB charging ports, offering visitors and employees an easy and convenient way to charge and power USB devices. Some USB outlets even offer battery backup, helping ensure that employees can charge their devices even in an instance of a power failure.
Littelfuse at Work
Protects input power stage and downstream components from overcurrent faults
Protects power unit from voltage surges
Rectification and blocking in power supply units
High switching speed in power supply units
Smart-Lighting Solutions
Smart lighting is a massive trend in commercial design — from office buildings to airports to parks to stadiums. Utilizing LEDs that offer significant power savings over traditional light bulbs, presence sensing to reduce unnecessary energy consumption, and networked systems to decrease maintenance costs, today’s lighting solutions are a significant point of savings in commercial applications.
Littelfuse at Work
Overcurrent protection
Primary surge protection
Transient voltage suppression
Bypass LED fail-open
GFCI/AFCI Receptacles
Not only are ground-fault circuit-interrupter outlets required by building code, they
are critical for protecting sensitive equipment and expensive computers. When a GFCI/AFCI outlet detects a suspected ground fault or arc, it interrupts power, helping keep devices safe and preventing potentially hazardous overcurrent situations.
Littelfuse at Work
Protects input power stage and
downstream components from overcurrent
MOV
Protects sensitive electronic components from voltage transients
Triggers electromechanical relay to disengage electrical contacts during fault
Intelligent Outlets
Intelligent outlets work with the building’s network to enable remote control
of devices plugged into the outlet via smartphone. These enable workers to remotely control any device plugged into the outlet.
Littelfuse at Work
Protects input power stage and
downstream components from overcurrent
Protects power unit from voltage surges
Schottky Diode
TVS Diode Array
Electronic Dimmers
Electronic dimmers control light levels using a solid-state MOSFET and are often internet-enabled. Electronic dimmers are helping commercial spaces save energy and reduce unnecessary lighting in rooms where no workers are present.
Littelfuse at Work
Protects input power stage and downstream components from faults
TRIAC
Gate Drive
Turns power supply units on and off
Electric, Gas, and Water Meters
Smart energy management starts at the source — in this case, electric, gas, and water meters. Smart meters are enabling a new standard of advanced energy management. By sending meter readings to the power, gas, or water utility wirelessly, utility companies can better understand consumption habits and plan accordingly. Smart meters can also enable building supervisors to better understand their energy, water, and gas consumption and find areas for improvement.
Littelfuse at Work
Cartridge Fuse
MOSFET/SiC MOSFET
Solid-State Relay
PIR Motion Detection
Passive infrared motion detectors have become the go-to standard for motion detection systems, not only used for security monitoring but also as occupancy detectors. With an ideal combination of performance and affordability, PIR motion detectors are ideally suited for applications where reliability and budget are a top concern.
Littelfuse at Work
AC/DC power stage
Motion detection
Reed Relay
Microcontroller unit
Smart Thermostats
While smart thermostats have quickly become commonplace in homes, businesses of all kinds are employing this technology to reap massive benefits and energy savings. These internet-capable devices have not only enabled easy remote control of a building’s temperature but are leveraging artificial intelligence and machine learning to understand temperature-setting trends
and better optimize HVAC systems for peak energy performance.
Littelfuse at Work
Power unit protection from overcurrent
Latching relay driver
Rechargeable battery-cell protection
Protects ICs from static discharge
HVAC Systems
If smart thermostats are the front end of temperature efficiency for building comfort, the HVAC systems themselves are the back end, where commercial buildings realize massive savings in energy. For both the HVAC control units and drive systems, Littelfuse products are helping to ensure that these systems operate reliably and safely and deliver peak performance.
Littelfuse at Work
Converts AC line voltage to DC
Switching power supplies
Protects HVAC system from overload and short-circuits
Isolation switch
Elevator and Escalator Systems
For decades, transport inside buildings remained relatively unchanged. Today, however, these systems are seeing a facelift in light of technological advances. Elevator and escalator drive systems are becoming smarter and more efficient, while elevator cabin solutions are making it easier for occupants to find their way around and give appropriate users access to the correct floors.
Littelfuse at Work
Provides open and close control signals to the electronic panel
Elevator load control
IGBT Module
Selective coordination and shunt-trip disconnection
New technology is helping security professionals deploy cameras that are smarter, more reliable, and better able to detect potential security threats. Littelfuse technology is inside today’s modern security cameras, especially in instances where robustness and reliability are critical. Advancements in wireless technology have also made wireless security cameras a more reliable standard, even with high-definition video. Littelfuse technology helps keep these security-critical devices protected.
Temperature sensing
PolySwitch PPTC
IGBT gate protection
Protects semiconductor devices in inverter
Protects Wi-Fi chipset from static discharge
Protects touchscreen ICs from static discharge
Polymer ESD Suppression
Reed Switch and Magnetic Actuator
Detects lock tampering
Open/closed proximity detection
Protects the unit from lightning or voltage transients
TVS Diode
Fuse
Protects touchscreen ICs from static discharge
Reed and Magnetic Actuator
Polymer ESD Suppression
MOV
Protects sensitive electronic components from voltage transients
Protects equipment and personnel from overcurrent
TVS Diode Array
Protects Wi-Fi chipset from static discharge
Protects power stage from overcurrent
Protects power unit from voltage transients and lightning
Optically isolated switch to drive motor
Protects USB-C plugs and receptacles from overheating
Protects power unit from voltage transients
Fuse
MOV
Solid-State Relay
Temperature Indicator
TVS Diode
Fuse
MOV
Schottky Diode
MOSFET
NTC
Fuse
MOV
SIDACtor + MOV
LED Protectors
Fuse
Protects power unit from voltage surges
TVS Diode
SCR
Fuse
MOV
Rectification and block in power supply units
Protects wireless chipset from static discharge
Fuse
AC switching for dimming light
Low-side gate driver for power MOSFETs
MOSFET
Protects power stage from overcurrent
Provides high-frequency load switching
Prevents magnetically induced tampering
Protects power stage from overcurrent
®
TVS Diode
PIR Sensor
Alarm
ZMOTION™
Chip Fuse 24 VAC
Solid-State Relay
Strap PPTC
TVS Diode Array
Rectifier Module
IGBT Module
TVS Diode
High-Speed Fuse
UL Class Fuses
Solid-State Relay
Reed Switch
Solid-State Relay
Switching power supplies
Elevator Shunt-Trip Disconnect Switch
commercial building and discover the ways Littelfuse is bringing the future of technology to today’s workplaces.
Provides isolation from MCU for pulse-out signal
Reed Switch
Application Block Diagram
Smart Locks
Application Block Diagram
Door and Window Sensors
Application Block Diagram
Outdoor and Wireless Security Cameras
Application Block Diagram
USB Outlets
Application Block Diagram
Smart-Lighting Solutions
Application Block Diagram
GFCI/AFCI Receptacles
Application Block Diagram
Intelligent Outlets
Application Block Diagram
Electronic Dimmers
Application Block Diagram
Electric, Gas, and Water Meters
Application Block Diagram
PIR Motion Detection
Application Block Diagram
Smart Thermostats
Application Block Diagram
HVAC Systems
Application Block Diagram
Elevator and Escalator Systems
Learn More